DIO.STATES

Description

DIO.STATES reads the states of the bi-directional I/Os. Each bit corresponds to a digital state. Bit 0 = DIO1 ... Bit 5 = DIO6.

Examples

Usage

When DIO1 and DIO3 are active (DIO#.STATE = 1). Bits 0 and 2 would be set. DIO.STATES would be 5.

Code

--> DIO.STATES
5

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only
Units N/A
Range 0 to 63
Default Value N/A
Data Type Integer
See Also  

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

DIO.STATES

3680h

00h

Unsigned32

-

-

Read only

Yes

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

DIO.STATES

2701

A8D

Unsigned32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

DIO.STATES

2701

Unsigned32

Read Only

-